Hello,
if external I2S bit clock enter MCLK pin of AIC3254, could AIC3254 sync I2S data successfully and don't need via Bit clock pin of aic3254? If could use MCLK pin for audio source clock, how to implement this function? Thank you.
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
if external I2S bit clock enter MCLK pin of AIC3254, could AIC3254 sync I2S data successfully and don't need via Bit clock pin of aic3254? If could use MCLK pin for audio source clock, how to implement this function? Thank you.
BR
Patrick
Hi, Patrick,
Assuming the operation of the device is Slave I²S mode, the application you mention is not possible as a Bit clock is required.
I think you are trying to configure the part to use a 3-wire I²S interface, if that is the case, the correct way to implement this will be to generate the internal system clock from the clock on BCLK pin instead of MCLK pin, so a clock in MCLK will not be required.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer