Part Number: SRC4193
Other Parts Discussed in Thread: SRC4192,
Will the SRC4193 or SRC4192 work with a 16 bit I2S input? The documentation is a little confusing. It talks generally about working with 24 bit I2S and 24 bit left justified input, but doesn't specifically mention 16 bit I2S input. It specifically mentions 16 bit right justified. Is this because the device determines the actual number bits from the width of the LRCLK? My application requires 16 bit I2S input in slave mode at 48KHz in a 16 bit frame resampled to 16 bit I2S output at 48 KHz in master mode (I'm trying to sync up an audio input with a 12.288MHz master clock generated by a processor).