I cannot achieve a 2.1VRMS full scale Analog Output signal from a 1KHz full source.digital media (USB (.mp3)/DVD Created my own media/CD (Converted the .MP3 to CD) I can output 2.0V RMS but is clipping, the best unclipped output is 1.77V RMS. Is that the best I should expect? Or is something wrong. I have a solid 1.8V and 3.3V DVDD. Any advise?
Thanks