Other Parts Discussed in Thread: PCM4204
When using PCM4204 EVM development board TDM mode, the board is configured as S/M=1, FMT2=0, FMT1=1, FMT2=1; /EXT=1, OSC1=0, OSC2=0; then FS2=0 , FS1 = 0, FS2 = 1 (Dual Rate), the acquisition frequency is set to 96K, LRCK = 96k, BCK = 24.576M, SCKI = 24.576M, but the ADC has no data output, but will FS2 = 0, FS1 = 0, FS2 = 0 (Singie Rate only supports up to 54K), the acquisition frequency is set to 96K, LRCK = 96k, BCK = 24.576M, SCKI = 24.576M, ADC has data output, but the data is not right! According to the description in the manual, and 96k need to be configured as FS2 = 0, FS1 = 0, FS2 = 1 only, can now be configured as FS2 = 0, FS1 = 0, FS2 = 1 no data output, please help support ,Thank you!