This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3268: AIC3268 interface

Part Number: TLV320AIC3268

Dear,

Could you help to confirm if we can set 2 IIS and 1 PCM with AIC3268?Thanks!

  • Hi, Sundy,

    I would like to clarify that PCM is the generic way to name digital audio stream like I²S, LJ or RJ. Are you referring to multi--channel transmission data (TDM)?.  As long as the sampling rate is the same among all the audio interfaces, this application is possible.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer

  • Diego,

    Do you mean if we want to transfer PCM formate data using 1 IIS interface ,we must set this IIS interface data rate the same as 2 other IIS?
    Thanks!
  • Hi, Sundy,

    Yes, if data is sent through the different interfaces, all of them should have the same sampling rate as the processing of the miniDSP runs under a single clock for all the interfaces.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer