This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6133A2: Need TPA6133's Output Current Limit Specification

Part Number: TPA6133A2


Hi Sirs,

Would you pls advise the output current limit specification of the TPA6133 since the 4mA~6mA data is an application example not this device's specification.
With 138mW, 16ohm load condition, we assume its current limit number should be at least 100mA.



Thanks a lot,

Wayne Chen
03/16/2018