This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3254: The S/N Value is distorted

Part Number: TLV320AIC3254


Hi Expert,

 I am debuging TLV320AIC3254 in sport DV,but after I tested the performance of TLV320AIC3254,I find the S/N value is  distorted.

Could you help to check it and give some suggestions?

Thanks a lot.

The test report is  as follows.

Test Project

■【Audio Test 

instrumentation Audio Precision,loudspeaker box
Test condition:Environmental noise<30DB  ,1KHZ,0DB sound source, the distance between sound source and product is 20cm,auido test software :AP2007.3.30

Test item Specifications and standards The test results determine
1#
1.
Sensitivity 
1.Make the horizontal distance between loudspeaker box and the Mic of DVT 30cm.
2.Play 1KHz/0dB sound source with loudspeaker box,adjustment output SPL and make it 72dBrA when 30cm far from the loudspeaker box.DVT REC the sound at the same time.
3.Connect DVT to Audio Precision 2722,and playback the video that recorded before.
4.Run the firmware of Audio Precision 2722 on PC,then we can get the output SPL.
Sensitivity
=20lg[Output Voltage(mV)/Input Voltage(mV)]
=Output SPL(dB)-input SPL(dB)
Criterion of Sensitivity:≥50dB(安霸),≥48dB(联咏)
50.606dB OK
2.
THD+N ratio
1.Make the horizontal distance between loudspeaker box and the Mic of DVT 30cm.
2.Play 1KHz/0dB sound source with loudspeaker box,adjustment output SPL and make it 72dBrA when 30cm far from the loudspeaker box.DVT REC the sound at the same time.
3.Connect DVT to Audio Precision 2722,and playback the video that recorded before.
4.Run the firmware of Audio Precision 2722 on PC,then we can get the info of THD+N.
Criterion of THD+N:<5%(安霸),<7%(联咏)
4.68% OK
3.
S/N
(录音信噪比)
1.Make the horizontal distance between loudspeaker box and the Mic of DVT 30cm.
2.Play 1KHz/0dB sound source with loudspeaker box,adjustment output SPL and make it 72dBrA when 30cm far from the loudspeaker box.DVT REC the sound at the same time.
3.Connect DVT to Audio Precision 2722,and playback the video that recorded before.
• Run the firmware of Audio Precision 2722 on PC,and push F4 button when the 1KHz being playbacked.Then we can get the info of SNR
Criterion of S/N:≤-30dB(安霸/联咏)
 -26.641dB NG

 

Test Pictures:

 

  • Hi, Rory,

    Welcome to E2E, Thanks for your interest in our products!.

    I am afraid the test information is not clear, is this test being done in the end-system?. Can you please also specify the block of the 'AIC3254 that is being measured (ADC, DAC, etc)?. The pictures seem to be corrupt, can you please re-upload them?.

    The test method seems related to the end-system, so it is possible that the issue with the signal to noise ratio is not related to the codec.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer