Hello together, I got stucked with my PCM9211.
I did manage to play audio from the ADC to MPO0, but I'm not able to get any sound output from an I2S source. I tried many different configurations and register-settings, but neither of them worked.
I'm using a bare PCM9211 (without EVM), default-config should be MPIO_C -> Auxin1 -> DIT -> MPO0, shouldn't it? Do I have to do anything else than putting the 4 wires of the source to MPIO_C to get SPDIF on MPO0?
Nevertheless, which input I chose in register 37h, I get "Out of range" (Only for ADC 38h shows 0x19 -> 48kHz), can I give you more information?
Thank you in advance,
regards Johannes