Part Number: TAS2557EVM
Other Parts Discussed in Thread: TAS2557, , PP-SALB2-EVM
Dear Sir,
I would like to demo TAS2557 to my customer. I had the EVM and PPC3 download.
I have problems (in PPC3) when using TAS2557EVM:
1) When I click Equalizer in Audio processing, error message pops up saying that Speaker SPL data is not present in selected characterization Data.
Unable switch on the SmartEq. (Please refer to attachment)
2) When above error message pops up, the software hang(no response when I click OK) and I need to force closing the software (by task manager). Is this normal?
3) I need to load ROM mode 1/2 in test and measurement, then playback music in media player then only there has sound output from the speaker.
Is this normal procedure?
4) Also, during initializing when click tuning and audio processing, there is error message at the end 'Failed to update process flow'. Is this OK?
Thanks.