Part Number: TPA3255
Hi,
if you put a low frequency sinewave into two devices,configured as PBTL and with same load,same external components, what is the max output phase delay difference between them?
Thanks
Umberto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPA3255
Hi,
if you put a low frequency sinewave into two devices,configured as PBTL and with same load,same external components, what is the max output phase delay difference between them?
Thanks
Umberto
Hi Umberto,
When using two devices in the same system, we recommend synchronizing the devices with the use of the oscillator pins. This allows one device to be the master and the other to be the slave. This will have a guaranteed phase delay between the two amplifiers. Please take a look a the 10.2.1.2.4 section of the TPA3255 data sheet and the Multi-Device Configuration for TPA32xx Amplifiers application note.
Justin