This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5121: Code example for configuration

Guru 16770 points

Part Number: PCM5121
Other Parts Discussed in Thread: PCM5242

Hi

1.

PCM5121 datasheet says a code example is provided in SLASE12.

SLASE12 is datasheet of PCM5242, but code example is not lined there.

Could you please share the code example?

2.

According to the following description of datasheet page 46, Auto Clock Configuration bit is set page0/register 0x25.

"When the Auto Clock Configuration bit is set (Page 0/ Register 0x25), no additional clocks configuration is required."

Is auto clock configuration bit equal to  DCAS?

3.

Default setting of DCAS should be 0.

So default settings indicate that manual PLL settings by user is invalid.

Is it correct?

BestRegards