Hi,
The datasheet specifies sampling rates of 32, 44.1, and 48 --- what determines the sampling rate? Can I set the device to work at, say, 48kHz no matter what?
I tried a circuit essentially identical to that in Figure 37 (section 10.2.3) in the datasheet, and I connected the I2S output to a DSP chip (the ADAU1701 evaluation board).
When I connect it to an Ubuntu Linux host, the generated I2S runs at 44.1kHz. Do I have control over the frequency to select 48kHz operation?
Thanks,
Carlos
--