This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2903B THD+N specification

Other Parts Discussed in Thread: PCM2903B

In the specification for the PCM2903B the THD+N figure at -1dB is specified in the Electrical Characteristics table as 0.01% typ for the ADC, with a note stating that it was measured using an audio test setup. However, in the graphs for the ADC THD+N at -1dB the figure looks more like 0.006%. Why is there a discrepancy between these two sets of figures? No doubt I'm missing something obvious:-)