This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM9211: Behavior When PCM9211 Detects DIR Errors

Part Number: PCM9211


Hi,

The ADC output is routed to the Main Output Port automatically after the wait time which is set to XTIWT[1:0] when the DIR is unlocked, so could you please tell me whether ADC output is routed to the Main Output Port even if setting 200ms to XTIWT[1:0] when the DIR is unlocked for only a short time(e.g. : 1ms) ?
I expect that the output will not be changed in above case.
In addition, could you please tell me the detailed detection algorithm that the DIR detects unlocking ?

Best regards,
Kato