Tool/software: Linux
Hello,
I want to play audio on Beaglebone black so i am using audio cape with TLV320AIC3106 codec for the same.I am able to load BB-BONE-AUDI-02-00A0.dtbo on 8.7 Debian(4.4 kernel) on Beaglebone Black as shown below. This BB-BONE-AUDI-02-00A0.dtbo file comes by default in the lib/firmware folder. i dint do any modifications in the .dtbo file.
8.7 debian IoT( 4.4.54-ti-r93 kernel)::
aplay -l ---> no devices found
After changing uEnv.txt (cape_enable=bone_capemgr.enable_partno=BB-BONE-AUDI-02)
root@beaglebone:~# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: B [AudioCape Rev B], device 0: davinci-mcasp.0-tlv320aic3x-hifi tlv320aic3x-hifi-0 []
Subdevices: 1/1
Subdevice #0: subdevice #0
**** List of PLAYBACK Hardware Devices ****
card 0: B [AudioCape Rev B], device 0: davinci-mcasp.0-tlv320aic3x-hifi tlv320aic3x-hifi-0 []
Subdevices: 1/1
Subdevice #0: subdevice #0
root@beaglebone:~# dmesg | grep cape
[ 0.000000] Kernel command line: console=ttyO0,115200n8 bone_capemgr.enable_partno=BB-BONE-AUDI-02 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait
[ 3.640488] bone_capemgr bone_capemgr: Baseboard: 'A335BNLT,00C0,4717BBBK0E43'
[ 3.647847] bone_capemgr bone_capemgr: compatible-baseboard=ti,beaglebone-black - #slots=4
[ 3.694039] bone_capemgr bone_capemgr: slot #0: No cape found
[ 3.738032] bone_capemgr bone_capemgr: slot #1: No cape found
[ 3.782031] bone_capemgr bone_capemgr: slot #2: No cape found
[ 3.826031] bone_capemgr bone_capemgr: slot #3: No cape found
[ 3.831847] bone_capemgr bone_capemgr: enabled_partno PARTNO 'BB-BONE-AUDI-02' VER 'N/A' PR '0'
[ 3.840606] bone_capemgr bone_capemgr: slot #4: override
[ 3.845962] bone_capemgr bone_capemgr: Using override eeprom data at slot 4
[ 3.852977] bone_capemgr bone_capemgr: slot #4: 'Override Board Name,00A0,Override Manuf,BB-BONE-AUDI-02'
[ 3.862957] bone_capemgr bone_capemgr: initialized OK.
[ 3.870580] bone_capemgr bone_capemgr: slot #4: dtbo 'BB-BONE-AUDI-02-00A0.dtbo' loaded; overlay id #0
[ 0.000000] Kernel command line: console=ttyO0,115200n8 bone_capemgr.enable_partno=BB-BONE-AUDI-02 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait
[ 3.640488] bone_capemgr bone_capemgr: Baseboard: 'A335BNLT,00C0,4717BBBK0E43'
[ 3.647847] bone_capemgr bone_capemgr: compatible-baseboard=ti,beaglebone-black - #slots=4
[ 3.694039] bone_capemgr bone_capemgr: slot #0: No cape found
[ 3.738032] bone_capemgr bone_capemgr: slot #1: No cape found
[ 3.782031] bone_capemgr bone_capemgr: slot #2: No cape found
[ 3.826031] bone_capemgr bone_capemgr: slot #3: No cape found
[ 3.831847] bone_capemgr bone_capemgr: enabled_partno PARTNO 'BB-BONE-AUDI-02' VER 'N/A' PR '0'
[ 3.840606] bone_capemgr bone_capemgr: slot #4: override
[ 3.845962] bone_capemgr bone_capemgr: Using override eeprom data at slot 4
[ 3.852977] bone_capemgr bone_capemgr: slot #4: 'Override Board Name,00A0,Override Manuf,BB-BONE-AUDI-02'
[ 3.862957] bone_capemgr bone_capemgr: initialized OK.
[ 3.870580] bone_capemgr bone_capemgr: slot #4: dtbo 'BB-BONE-AUDI-02-00A0.dtbo' loaded; overlay id #0
the logs show that BB-BONE-AUDI-02 overlay was loaded and i was also successfull in playing audio .i connected speaker as well so good quality sound is also coming
But when i tried enabling same audio cape on debian 9.3(4.9 kernel) using uboot-overlay method,its hanging while booting itself,not completing the booting.
9.3 debian IoT(4.9.82 kernel)::
uEnv.txt: (changes are underlined)
root@beaglebone:/sys/devices/platform/ocp# cat /boot/uEnv.txt
#Docs: http://elinux.org/Beagleboard:U-boot_partitioning_layout_2.0
#Docs: http://elinux.org/Beagleboard:U-boot_partitioning_layout_2.0
uname_r=4.9.82-ti-r102
#uuid=
#dtb=
#uuid=
#dtb=
###U-Boot Overlays###
###Documentation: http://elinux.org/Beagleboard:BeagleBoneBlack_Debian#U-Boot_Overlays
###Master Enable
enable_uboot_overlays=1
###
###Overide capes with eeprom
uboot_overlay_addr0=/lib/firmware/BB-UART1-00A0.dtbo
uboot_overlay_addr1=/lib/firmware/BB-BONE-AUDI-02-00A0.dtbo
#uboot_overlay_addr2=/lib/firmware/<file2>.dtbo
#uboot_overlay_addr3=/lib/firmware/<file3>.dtbo
###
###Additional custom capes
#uboot_overlay_addr4=/lib/firmware/<file4>.dtbo
#uboot_overlay_addr5=/lib/firmware/<file5>.dtbo
#uboot_overlay_addr6=/lib/firmware/<file6>.dtbo
#uboot_overlay_addr7=/lib/firmware/<file7>.dtbo
###
###Custom Cape
#dtb_overlay=/lib/firmware/<file8>.dtbo
###
###Disable auto loading of virtual capes (emmc/video/wireless/adc)
#disable_uboot_overlay_emmc=1
#disable_uboot_overlay_video=1
disable_uboot_overlay_audio=1
#disable_uboot_overlay_wireless=1
#disable_uboot_overlay_adc=1
###
###PRUSS OPTIONS
###pru_rproc (4.4.x-ti kernel)
#uboot_overlay_pru=/lib/firmware/AM335X-PRU-RPROC-4-4-TI-00A0.dtbo
###pru_uio (4.4.x-ti, 4.14.x-ti & mainline/bone kernel)
#uboot_overlay_pru=/lib/firmware/AM335X-PRU-UIO-00A0.dtbo
###
###Cape Universal Enable
enable_uboot_cape_universal=1
###
###Debug: disable uboot autoload of Cape
#disable_uboot_overlay_addr0=1
#disable_uboot_overlay_addr1=1
#disable_uboot_overlay_addr2=1
#disable_uboot_overlay_addr3=1
###
###U-Boot fdt tweaks... (60000 = 384KB)
#uboot_fdt_buffer=0x60000
###U-Boot Overlays###
#cmdline=coherent_pool=1M net.ifnames=0 quiet
#In the event of edid real failures, uncomment this next line:
#cmdline=coherent_pool=1M net.ifnames=0 quiet video=HDMI-A-1:1024x768@60e
#cmdline=coherent_pool=1M net.ifnames=0 quiet video=HDMI-A-1:1024x768@60e
##enable Generic eMMC Flasher:
##make sure, these tools are installed: dosfstools rsync
#cmdline=init=/opt/scripts/tools/eMMC/init-eMMC-flasher-v3.sh
##make sure, these tools are installed: dosfstools rsync
#cmdline=init=/opt/scripts/tools/eMMC/init-eMMC-flasher-v3.sh
root@beaglebone:~# aplay -l
aplay: device_list:270: no soundcards found...
aplay: device_list:270: no soundcards found...
i tried adding BB-UART1 as well using uboot-overlay,so boot logs tell uart1 got loaded properly.
uboot_overlays: loading /lib/firmware/BB-UART1-00A0.dtbo ...
1075 bytes read in 222 ms (3.9 KiB/s)
But when i tried the same with audio cape,the booting hangs in between as shown below in the boot logs:
ERROR: Did not find a cmdline Flattened Device Tree
Could not find a valid device tree
** Invalid partition 2 **
** Invalid partition 3 **
** Invalid partition 4 **
** Invalid partition 5 **
** Invalid partition 6 **
** Invalid partition 7 **
switch to partitions #0, OK
mmc1(part 0) is current device
Scanning mmc 1:1...
gpio: pin 56 (gpio 56) value is 0
gpio: pin 55 (gpio 55) value is 0
gpio: pin 54 (gpio 54) value is 0
gpio: pin 53 (gpio 53) value is 1
switch to partitions #0, OK
mmc1(part 0) is current device
Could not find a valid device tree
** Invalid partition 2 **
** Invalid partition 3 **
** Invalid partition 4 **
** Invalid partition 5 **
** Invalid partition 6 **
** Invalid partition 7 **
switch to partitions #0, OK
mmc1(part 0) is current device
Scanning mmc 1:1...
gpio: pin 56 (gpio 56) value is 0
gpio: pin 55 (gpio 55) value is 0
gpio: pin 54 (gpio 54) value is 0
gpio: pin 53 (gpio 53) value is 1
switch to partitions #0, OK
mmc1(part 0) is current device
uboot_overlays: loading /lib/firmware/BB-UART1-00A0.dtbo ...
1075 bytes read in 222 ms (3.9 KiB/s)
1075 bytes read in 222 ms (3.9 KiB/s)
uboot_overlays: loading /lib/firmware/BB-BONE-AUDI-02-00A0.dtbo ...
2859 bytes read in 306 ms (8.8 KiB/s)
failed on fdt_overlay_apply(): FDT_ERR_NOTFOUND
uboot_overlays: loading /lib/firmware/BB-BONE-eMMC1-01-00A0.dtbo ...
1440 bytes read in 373 ms (2.9 KiB/s)
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
failed on fdt_overlay_apply(): FDT_ERR_BADMAGIC
base fdt does did not have a /__symbols__ node
make sure you've compiled with -@
uboot_overlays: cape universal disabled, external cape enabled or detected...
loading /boot/initrd.img-4.1.15-ti-rt-r43 ...
4096241 bytes read in 274 ms (14.3 MiB/s)
debug: [console=ttyO0,115200n8 bone_capemgr.uboot_capemgr_enabled=1 root=UUID=76ea7739-c46a-42c5-89e1-5dbb28d3a184 ro rootfstype=ext4 rootwait coherent_pool=1M quiet cape_universal=enable] ...
debug: [bootz 0x82000000 0x88080000:3e80f1 88000000] ...
ERROR: Did not find a cmdline Flattened Device Tree
Could not find a valid device tree
debug: [console=ttyO0,115200n8 bone_capemgr.uboot_capemgr_enabled=1 root=/dev/mmcblk1p1 ro rootfstype=ext4 rootwait coherent_pool=1M quiet cape_universal=enable] ...
debug: [bootz 0x82000000 0x88080000:3e80f1 88000000] ...
ERROR: Did not find a cmdline Flattened Device Tree
Could not find a valid device tree
** Invalid partition 2 **
** Invalid partition 3 **
** Invalid partition 4 **
** Invalid partition 5 **
** Invalid partition 6 **
** Invalid partition 7 **
starting USB...
USB0: Port not available.
link up on port 0, speed 100, full duplex
BOOTP broadcast 1
DHCP client bound to address 192.168.1.243 (4 ms)
Using cpsw device
TFTP from server 192.168.1.1; our IP address is 192.168.1.243
Filename 'vmlinuz-4.1.15-ti-rt-r43'.
Load address: 0x82000000
Loading: T T T T T T T T T T T T T T T T T T T T
Retry count exceeded; starting again
missing environment variable: pxeuuid
Retrieving file: pxelinux.cfg/01-98-5d-ad-ec-34-c4
link up on port 0, speed 100, full duplex
Using cpsw device
TFTP from server 192.168.1.1; our IP address is 192.168.1.243
Filename 'pxelinux.cfg/01-98-5d-ad-ec-34-c4'.
Load address: 0x80100000
Loading: T T T T T T T T T T T T T T T T T T T T
failed on fdt_overlay_apply(): FDT_ERR_NOTFOUND
uboot_overlays: loading /lib/firmware/BB-BONE-eMMC1-01-00A0.dtbo ...
1440 bytes read in 373 ms (2.9 KiB/s)
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
failed on fdt_overlay_apply(): FDT_ERR_BADMAGIC
base fdt does did not have a /__symbols__ node
make sure you've compiled with -@
uboot_overlays: cape universal disabled, external cape enabled or detected...
loading /boot/initrd.img-4.1.15-ti-rt-r43 ...
4096241 bytes read in 274 ms (14.3 MiB/s)
debug: [console=ttyO0,115200n8 bone_capemgr.uboot_capemgr_enabled=1 root=UUID=76ea7739-c46a-42c5-89e1-5dbb28d3a184 ro rootfstype=ext4 rootwait coherent_pool=1M quiet cape_universal=enable] ...
debug: [bootz 0x82000000 0x88080000:3e80f1 88000000] ...
ERROR: Did not find a cmdline Flattened Device Tree
Could not find a valid device tree
debug: [console=ttyO0,115200n8 bone_capemgr.uboot_capemgr_enabled=1 root=/dev/mmcblk1p1 ro rootfstype=ext4 rootwait coherent_pool=1M quiet cape_universal=enable] ...
debug: [bootz 0x82000000 0x88080000:3e80f1 88000000] ...
ERROR: Did not find a cmdline Flattened Device Tree
Could not find a valid device tree
** Invalid partition 2 **
** Invalid partition 3 **
** Invalid partition 4 **
** Invalid partition 5 **
** Invalid partition 6 **
** Invalid partition 7 **
starting USB...
USB0: Port not available.
link up on port 0, speed 100, full duplex
BOOTP broadcast 1
DHCP client bound to address 192.168.1.243 (4 ms)
Using cpsw device
TFTP from server 192.168.1.1; our IP address is 192.168.1.243
Filename 'vmlinuz-4.1.15-ti-rt-r43'.
Load address: 0x82000000
Loading: T T T T T T T T T T T T T T T T T T T T
Retry count exceeded; starting again
missing environment variable: pxeuuid
Retrieving file: pxelinux.cfg/01-98-5d-ad-ec-34-c4
link up on port 0, speed 100, full duplex
Using cpsw device
TFTP from server 192.168.1.1; our IP address is 192.168.1.243
Filename 'pxelinux.cfg/01-98-5d-ad-ec-34-c4'.
Load address: 0x80100000
Loading: T T T T T T T T T T T T T T T T T T T T
I guess on 8.7 debian i loaded the overlay using bone_capemgr/slots method but on new kernel, we dont have an option of adding overlays to slots file instead we have to add it to uboot-overlay method.So for doing that any modifications required in BB-BONE-AUDI-02-00A0.dts file? If yes ,can anyone please share that dts file and also help me with the modifications to be done? I have been stuck with this since a week,please help where am i going wrong.I couldnt find any support for loading audio cape on latest kernel. waiting for your response.
Thanks,
Jithu.
Thanks,
Jithu.