Part Number: PCM2912A
Hello,
I want to use an external 6MHz crystal OSC instead of a crystal resonator for the PCM2912A due to space constraints. The datasheet mentions they dont recommend this since you cant use sspnd to disable the clock. Accordingly to section 9.3.11.4 in the DS, the PCM2912A enters a suspend state when it sees a constant idle state on the USB bus after approximately 5 ms. Will there be any issue if we still have a 6MHz input clock during this suspend state?
Thanks,
Amy