Other Parts Discussed in Thread: TLV320ADC3101, , PCM1865
i use TLV320ADC3101 have no use MCLK in,
PCM1863/65 the SCKI is Must connect? THANKS!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Ray,
The PCM1863 and PCM1865 are devices which can operate in a 3-wire I²S mode, without a MCLK/SCKI master clock. This family of devices features an advanced automatic clock detection which can configure the PLL to generate an internal system clock for the device operation. The Automatic clock detection will work only with standard audio clocks. Please refer to section 9.3.9.4 of the datasheet for more details.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer