I'm trying to assign the device as a SPDIF receiver(1 coaxial & 1 optical) + I2S inputs (from 3 other sources),through the usual RXIN pins + MPIOs.
Looking through the datasheet,I can use AUX0,AUX1 & AUX2 for I2S inputs, but seems doesn't much info available on dealing with AUX0(RXIN4~RXIN7)as one of the I2S input.Is the function is not ready yet or something i missed?All control will be done using a I2C mcu.
Note that the I2S output will be the default main port output.