This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5122: PurePath - Unable to add components once PCM51XX is added

Part Number: PCM5122
Other Parts Discussed in Thread: PCM5142

hi,

I'm just starting out on using PurePath Studio, and when I add the PCM51XX ROM Framework to my Diagram, I can no longer add any other components. 

If I ad a PCM5142 framework it works fine, but I'm not sure that would work - are the PCM5142  / PCM5122 frameworks interchangeable?

  • Hi IceMan,

    Note that the PCM5122 does not have a full feature miniDSP. This device only has a ROM, so the flow is limited to the preset program. The user only has access to the coefficients for the static process flow. If you wish to modify the process flow, you will need to use the PCM5142 device and its framework.

    Thanks!
    Paul