Other Parts Discussed in Thread: PCM1861, PCM1865EVM, PCM1865
Could I use 12MHz CRYSTAL on the XO and XI Pin?
Will there be any problem?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could I use 12MHz CRYSTAL on the XO and XI Pin?
Will there be any problem?
Hi, Seven,
Welcome to E2E, Thanks for your interest in our products!.
The PCM1863 can operate with a 12MHz crystal, but please consider that the internal clock coefficients, dividers and PLL should be manually configured as the automatic clock configuration of the device does not work with non-audio standard clock frequencies.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi, Seven,
This device has a flexible clock tree, allowing the GPIO1 to output the system clock, which can effectively be the input SCKI, but if a different value is required and the PLL is used, the PLL output clock can be routed to a divider which can be used to divide the clock and setup an output clock of the desired frequency. I would recommend you to take a look to section 9.3.9.4.2 of the datasheet to find detailed information about the clocking configurations.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi, Seven
The values for the supported crystal frequencies of the PCM1861 comes from design specification. It is not possible to just change the minimum spec.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi, Seven,
That is the basic configuration required to use the interrupt function of the PCM1863. For a detailed implementation example, pelase refer to section 9.5.3 of the datasheet.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer