This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5717: TAS5717 BTL and PBTL with BD Modulation Codes Confirmation

Part Number: TAS5717


Hi Sirs,

Would you pls assist me to review of my proposal for TAS5717 BD modulation for BTL and PBTL modes?

BTL (stereo):

------------------------------------------

#Enable PLL

0x1B = 0x00

 

# BD Modulation

0x20 = 0x00 89 77 72

0x11 = 0xB8

0x12 = 0x60

0x13 = 0xA0

0x14 = 0x48

 

# Volume Control (0dB)

0x07 = 0x00C0

 

#Enable Amp

0x05 = 0x00

------------------------------------------

 

PBTL (mono, A+B, C+D):

------------------------------------------

#Enable PLL

0x1B = 0x00

 

# BD Modulation

0x20 = 0x00 89 77 72

0x11 = 0xB8

0x12 = 0x60

0x13 = 0xA0

0x14 = 0x48

 

# PBTL

0x19 = 0x3A

0x25 = 0x 01 00 22 45

 

# Volume Control (0dB)

0x07 = 0x00C0

 

#Enable Amp

0x05 = 0x00

------------------------------------------

Thank you and Best regards,

Wayne Chen
05/21/2018

  • Hi Wayne
    I think the confguration you shownn above is correct.
    Best regards,
    Shawn Zheng
  • Hello Shawn,

    Thanks for your advise. The CFG works on the EVM. I polished the PBTL instructions by adding mixer for mono output:

    -------------------------------------------------------------
    ! Enable PLL
    X1b 00

    ! BD Modulation
    X20 00 89 77 72
    X11 b8
    X12 60
    X13 a0
    X14 48

    ! Mixer Output = L+R
    X72 00 80 00 00
    X73 00 80 00 00
    X76 00 80 00 00
    X77 00 80 00 00

    ! PBTL Mode
    X19 3a
    X25 01 00 22 45

    ! Enable Class-D Amp
    X05 00

    ! Volume Control (Gain, 0x07=0x00c0=0dB)
    X07 00 c0
    -------------------------------------------------------------

    Thanks a lot

    Wayne Chen
    05/23/2018