This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5411-Q1: TAS5411 "turn on time" ???

Part Number: TAS5411-Q1

[#1] I can not find the "turn on time" in your TAS5411 datasheet. Can you please tell me or point me to the turn on time from -Standby negating until the output driver is valid and driving? 

[#2} Also, the text says the "load diagnostic function" runs on the de-assertion of STANDBY and takes 229mS to run.

     QUESTION:  Is there a way to disable this? My application needs to re-assert STANDBY very quickly after de-assertion and I can not wait 229mS.

[#3] Request: I am looking for an audio amplifier capable of delivering 1A with a 15V supply or higher.   I need turn on time ideally in the 2mS range.

               Can you recommend a device with these specs?