Part Number: TLV320AIC3104
Hi Team,
If 3104 pin LINE1LP used as single-ended input, how to deal with LINE1LM? If we can left LINE1LM pin floating?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV320AIC3104
Hi Team,
If 3104 pin LINE1LP used as single-ended input, how to deal with LINE1LM? If we can left LINE1LM pin floating?
Hi, Lilian,
If the inputs are configured to operate in Single-ended mode, it is recommended to connect LINE1LM to GND through a decoupling cap of the same value as the one connected in Line1LP.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi Diego,
What's the recommend decoupling cap value of input pin like Line1LP?
Thank you
HI, Lilian,
The selection of the input cap depends on the desired frequency response for the DC filter formed by the cap and input impedance. For this particular device, the input impedance changes with the input PGA mix setting, which varies from 20KΩ (0dB gain set) to 80KΩ (-12dB gain set). A typical value we recommend is 0.1µF of 0.47µF.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer