Part Number: TPA3136D2
Hi,
is there a way to disable the fault pin function on TPA3136D2?
see that the minimum differential input voltage required to trigger the DC detec is 130mV.
That means, if i have a 1kHz sine wave at 200mV Amplitude it will trigger the DC detec?
Is there a way to disable it or to increase this value?
My problem is that my output volume is too low and i have to increase the input amplitude.
But the 'FAULT' is connected to 'EN' and is shutting the IC down.
Why cant he handle higher amplitudes?(Should i increase the capacitor on inputs?)
Here is my schematic: