This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA4311EVM: PGA4311EVM

Part Number: PGA4311EVM


Who is the manufacturer and what are the part numbers of the connectors used on the PGA4311EVM board. I would like to use the board and use connectors that properly mate.  Thank you.

  • Hi Stephen,

    Which connector in particular were you wondering about? The audio inputs and outputs are standard RCA-style jacks. the control port to connect to a PC is a standard male DB-25 connector. Alternatively, the SPI bus and control signals are available on two 7x2 .100" male headers. All three connector types are fairly generic.

    Examples:

    DB-25F

    7x2 header 

    I can't think of a good way to handle the RCA jacks as a board-to-board connector. Those connections are pinned out as test points, so it may be easiest just to hard-wire them. 

  • Stephen

    We haven't heard back from you so we assume this answered your question. If not, post a reply below, or create a new thread if this one has timed-out.

    Thanks
    Dennis