Other Parts Discussed in Thread: TLV320AIC3120,
hi,
I am trying to generate beep of 2KHz for 2sec, but i am not getting the beep for 2sec it is less than the time expected.
My second question is that, although i have changed volume setting , I am not getting loud enough beep.
this is the setting configuration.
can you help me out for the same
Select Page 0
w 30 00 00
# PLL_CLKIN = MCLK, CODEC_CLKIN = MCLK
# MCLK=2,048000Hz
w 30 04 00
# DAC Instruction set PRB_P25
w 30 3C 19
# NDAC ON div=1
w 30 0B 81
# MDAC ON div=2
w 30 0C 82
# DOSR = 128
w 30 0D 00
w 30 0E 80
# DAC Volume -63.5 dB
w 30 41 81
# Select Page 0
w 30 00 00
# DAC mute off
w 30 40 04
# DAC power up
w 30 3F 80
# Select Page 1
w 30 00 01
# Class d driver power up
w 30 20 86
# Class D route enable
w 30 26 95
# Class D output driver mute off
w 30 2A 04
# Select Page 0
w 30 00 00
# Beep length=017700
w 30 49 01
w 30 4A 77
w 30 4B 00
# sin wave coff=23FB
w 30 4C 23
w 30 4D FB
# cos wave coff=7AD7
w 30 4E 7A
w 30 4F D7
# Beep generate -2dB
w 30 47 84
Thanks,
Zanza Bhatt