1. There is a pin on the 3107 chip called IOVDD that sets the logic high threshold. The choices for this are +1.8 and +3.3 VDC. The actual logic high threshold is 0.7 x IOVDD. The EVM board comes with this jumpered to +1.8 VDC. Is this the right value for our board where the 3107 is controlled by a dsPIC that is a 3.3V part?
2. On the 3107 EVM on the Left_LOP and Right_LOP line outputs there are RC filters (47-nF, 100-Ohm, 1-uF) --- are these important for us to include on our board design?
3. There is a difference in the Mic bias resistor values (2.2K vs 1K) and the Mic coupling cap values (0.47uF vs 0.1uF) between the page 18 of datasheet and the page 36 of EVM. Should I follow datasheet or EVM to get the highest microphone audio quality for speakerphone products?