Part Number: TPA3100D2
Can somebody tell me what should be the voltage on the speakers outputs of TPA3100D2 in BTL format, the supply voltage is about 24 volts. None of the speaker outputs is grounded or supplied through a capacitor.
Thanks
Satya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks, I mean what is the voltage expected on the output? In my experience the four outputs should show 8 or 9 volts on each of the pins. I have an amplifier whose ic TPA3100D2 appears to be not working and it shows 9 volts each on two of the outputs and zero on the other two.
I am trying to determine if the ic is defective or there is a defect in the parts connected to it.
The speakers have been tested and are OK.
Hello Shawn,
Thanks for your message. With audio being fed in,there are about 2.4 volts in three of the inputs, while the fourth has 3.4 volts. I can trace the audio in each of these inputs.
There is no capacitor but a resistor of 103 ohms feeding these inputs.
The two speaker outputs are showing 9 volts on one side EACH and zero on the other side, with speakers disconnected.
When I connect the speakers, the smps power supply goes to zero.
Do not have a circuit diagram otherwise would have sent you.
With best wishes.
Satya
Hi Saya,
Sounds like the DC block capacitors on the input are NOT used in your application, please add 1uF capacitors on the input. The Figure24 in the datasheet shows a typical application circuit for TPA3100D2.
Best regards,
Shawn Zheng
Thanks, let me see if I can do it. This ic runs the tweeters and there is a different ic which runs the woofer, but both are powered from same smps. Even the other ic does not have any
capacitor to to its input. The other ic and the woofer work, if I do not connect the tweeters to the ic.
With best wishes.
Satya
Thanks, I have today replaced this ic , but i am still not getting any sound in the speakers (tweeters) though now both sets of output pins show 7.6 volts with speakers connected.
As I had mentioned earlier previously the smps used to go to zero volts when speakers were connected, this is not happening now, with the new ic.
I am able to trace the audio into the input of the ic.
Unfortunately I do not have a schematic of this set.
With best wishes.
Satya
I forgot to mention that I tried to measure voltage at fault, mute and shutdown it shows zero volts. I tried to give voltage at shutdown but did not have any luck.
The voltage at vreg shows 4 volts.
With best wishes.
Satya
Hello Shawn,
Thanks, I made a mistake and can read about 3.1 volts on the shutdown, not sure if this is still too low.
With best wishes.
Satya
Hello Shawn,
Unfortunately I do not have a schematic. Also wanted to ask you the voltage on ROSC is 1.7 and shows a resistance of about 35 K. The VBYP shows 1.2 volts.
I think the speakers pinout voltage which show about 7.6 on both are a little low, I believe it should be half of powers supply.
With best wishes.
Satya
Hi Shawn,
I am getting about 11.7 volts on BSRP, BSLP etc. and only 7.6 on the output pins. Is the voltage for BSRP etc. OK?
Best regards.
Satya
Hi Shawn,
You are right the supply voltages is 24. I do not have a scope to check the waveform.
Can you tell me what should be the voltage at MSTR/SLV if I want to run it by itself, as master?
Kind regards
Satya