Other Parts Discussed in Thread: TPA6204A1, TPA6211A1
I need to interface to a device/product that uses a TPA2010D1 as the audio amp which feeds connections to the outside world. I cannot change that. The + and - outputs are available to me directly (no speaker or other load is connected). I do not want, and do not need all of the power this output can provide, rather I need to essentially just tap off of it a small level to feed some other audio processing circuitry and I would REALLY like to connect to just one side (prefer the minus side). I realize that at a minimum I will probably need a blocking cap but what else should I be concerned about? Do I need to load the unused side (plus) with a similar load as my connection on the minus side?
Thanks,
Phil