Part Number: PCM1865
Hello
when we set the 2 PCM1865 Devices as 8 Channel TDM mode, which rigsters need to be setting ? and is there other configurations need to set?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Jesse,
The PCM1865 can be configured for TDM mode with 8 channels, the basic register configuration is mentioned below.
One thing to note is that for TDM mode, the PCM1865 only accepts a BCLK of 256×Fs.
For additional information about the TDM operation of the PCM186x devices, please refer to section 9.3.16.4 of the latest datasheet.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer