This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2560: VREG output?

Part Number: TAS2560


Hi Expert,

The project used TAS2560, but I2C can't get the ACK, I want to check the peripheral circuit, what's should I get voltage from VREG? (VBAT=4.0V)

Anything I can check for it? Thanks!

  • Hi Jerry,

    I took some measurements on the EVM: In idle state (device not configured) and VBAT = 4V, VREG is around 3.68V. With the device configured, VREG goes up to around 7V.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators