I am using PPC3 with LB2 connected to TAS2555YZEVM. I perform the hardware checks and do a speaker fit test. No problems. However when I run the speaker excursion test to determine Bl, I get a fit error. The displacement curve is not seen or displayed.
I have checked the excursion signal at the BNC connector with a scope and it looks fine. The EVM is not seeing signal.