Part Number: PCM5242
Hello,
I have a new design. The design requires the option for both Single Ended and Differential to work at the same output pins. I plan on integrating the low-pass filter as described on page 44 Figure 66. I also appreciate the ESD protection it provides.
Does the following filter allow for a single ended connection to be simply connected to the + pins of the left/right channels? Or does this filter require a differential connection at the output when used. It says in the datasheet "The PCM5242 can also support single ended outputs, using OUTLP and OUTRP respectively. A single 470Ω and 2.2nF capacitor can be used on each pin in single ended mode". This circuit is slightly different than that. But will it work as an "optional differential/single ended" output?
Is it possible to connect both single ended and differential devices to this exact same circuit? What about if this happens at the same time? Would that be a problem? Does this require a differential to single ended conversion? I hope not. This would be easier! :-)
Thanks for the help!
Jay