Part Number: TLV320AIC3256
Channel 1 is MIC input. SE in. external MIC bias.
Channel 2 is BT speaker. Diff. in.
below is my register table, please help me check any wrong?
when i only channel 1 or only channel 2 input, there is no any noise.
but when i both Ch1 & Ch2 input, there is noise issue here.
static const RegValue RecordingBothOn[] = {
//{0x00, 0x01}, //# switch to page1
//{0x33, 0x40}, //# Enable MICBIAS and set to 1.25V, MICBIAS voltage is generated from AVDD
{0x00, 0x00},
{0x3D, 0x01},
{0x00, 0x01},
{0x01, 0x08},
{0x02, 0x00},
{0x3D, 0x00},
{0x47, 0x32},
{0x7B, 0x01},
{0x00, 0x01},
{0x33, 0x00}, //40
#ifdef CONFIG_TARGET_BOARD_R1_PRO
// {0x34, 0x33}, //# IN1R, IN2L is routed to Left MICPGA POSITIVE with 40K resistance
// {0x36, 0xF0}, //# IN2R CM1L, is routed to Left MICPGA NEGATIVE with 40K resistance
// {0x37, 0xF0}, //# IN1R, IN2R is routed to Right MICPGA POSITIVE with 40K resistance
// {0x39, 0xCC}, //# , CM1L is routed to Right MICPGA NEGATIVE with 40K resistance
//{0x34, 0x22}, //# IN1R, IN2L is routed to Left MICPGA POSITIVE with 40K resistance
//{0x36, 0xA2}, //# IN2R CM1L, is routed to Left MICPGA NEGATIVE with 40K resistance
//{0x37, 0xA2}, //# IN1R, IN2R is routed to Right MICPGA POSITIVE with 40K resistance
//{0x39, 0x82}, //# , CM1L is routed to Right MICPGA NEGATIVE with 40K resistance
//{0x34, 0x02}, //# only mic /20K
//{0x36, 0x82}, //#
//{0x37, 0x80}, //#
//{0x39, 0x82}, //#
//{0x34, 0x20}, //# only BT /20K
//{0x36, 0x20}, //#
//{0x37, 0x22}, //#
//{0x39, 0x00}, //#
{0x34, 0xf3}, //0x55 //0x8a
{0x36, 0xf3},
{0x37, 0xf3}, //0x44 //0x88
{0x39, 0xf3},
#endif
#ifdef CONFIG_TARGET_BOARD_10C_EVO
#if 0 // 20K
{0x34, 0x0A}, //# IN1R, IN3L is routed to Left MICPGA POSITIVE with 40K resistance
{0x36, 0x8A}, //# IN3R, CM1L, is routed to Left MICPGA NEGATIVE with 40K resistance
{0x37, 0x88}, //# IN1R, IN3R is routed to Right MICPGA POSITIVE with 40K resistance
{0x39, 0x8A}, //# IN3L, CM1L is routed to Right MICPGA NEGATIVE with 40K resistance
#else // 40K
{0x34, 0x0F}, //# IN1R, IN3L is routed to Left MICPGA POSITIVE with 40K resistance
{0x36, 0xCF}, //# IN3R, CM1L, CM2L is routed to Left MICPGA NEGATIVE with 40K resistance
{0x37, 0xCC}, //# IN1R, IN3R is routed to Right MICPGA POSITIVE with 40K resistance
{0x39, 0xCF}, //# IN3L, CM1L, CM2L is routed to Right MICPGA NEGATIVE with 40K resistance
#endif
#endif
{0x3B, 0x28}, //# Left MICPGA Gain is enabled, Left MICPGA Gain is set to 0dB 08
{0x3C, 0x28}, //# Right MICPGA Gain is enabled, Right MICPGA Gain is set to 0dB 08
{0x00, 0x00}, //# Select Page 0
{0x53, 0x00}, //# Left ADC Channel Volume = 10dB 14
{0x54, 0x00}, //# Left ADC Channel Volume = 10dB 14
{0x51, 0xC0}, //# Power up LADC, Power up RADC
{0x52, 0x00}, //# Unmute LADC, Unmute RADC
};