Other Parts Discussed in Thread: TPA3113D2
Hi,
We are using audio codec TLV320AIC3254-Q1 and we need to connect two 5W speakers with 8 ohms to it. So we choose Audio Power Amplifier TPA3113D2 which has two outputs.
We have some concerns regarding the interface.
Input impedance of audio amplifier is configurable and its lowest value is 9 K ohms. In audio codec output impedance of LOL & LOR is 10 K ohms and HPL & HPR has 32 Ohms as maximum impedance.
Does this two have to match? If yes, how can we match these impedance (output of codec to input of amplifier)
Regards,
Francy Babu