Hi,
I have a simple recording and playback setup that is working with the AIC3262App2x1x framework but I would like to switch to the AIC3262App8x4x framework in order to get more DSP cycles for doing more complex processing. However when I switch to the 8x4x framework my audio out works fine but the audio in only produces noise. I'm assuming the sample rates need adjusting somewhere but I haven't been able to figure out where from the documentation. I have a digital MIC input and a 48kHz I2S output (fixed). The setup is as below: