Other Parts Discussed in Thread: TLV320AIC3106
Hello TI Community,
I recently got TLV320AIC3106EVM-K devkit and it seems to be having some serious hardware issues.
My setup is: [LINE OUT (PC DAC)] -> [LINE2 R IN (TLV board)] -> [HEADSET output]
It is detected by Windows and TLV320AIC310xEVM Evaluation Tool without a problem, but after trying couple configuration I was unable to make it work.
After couple of unfruitful trials I checked the temperature on TLV chip and it turned out to be burning hot. I've also checked levels on 5V and 3.3V testpoints and there is no voltage. It's worth mentioning that I made sure all jumpers were placed in their default positions. Also, according to troubleshoot instruction, D6 should be ON, but it's always OFF.
Do You have any solution to this problem? I am worried that TLV chip may be fried because of such high temperatures.
Kind regards
Jakub