Part Number: PCM1865EVM
Other Parts Discussed in Thread: PCM1865, PCM9211
Hello
We have recently bought a pcm1865evm and request PPC2 console to test it on a windows machine. However, I am not bale to work with PPC2 GUI properly.
I connect the 4-channel stereo input to analogue audio signals and then connect the optical output to a Hammerfall DSP Multiface (HDSP) mixer according to the user guide information (page 13).
However, I only see two channels in the HDSP mixer by setting the mode of the pcm1865evm to 0.
In mode 1 and 2 I do not see any audio. For mode 2 it is correct, however, for mode 1 I should be able to process 4 channels!!
- Overall, how can I get this device to work on a windows machine and record a 4-channel audio signals?
- Is the board able to record 8 channel mono signals?
Bets regards
Mehdi