This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS1020 USB to AC97 interface

Dear all,

On a new board, I search one way to interface one AC97 audio codec with one host pc by USB. I take a look on the TAS1020 and I think it can make that.

but if I connect the TAS1020 to an AC97 codec, can I access to all functions of the codec with its driver (provide by the AC97 vendor) or must I write some driver or application for the TAS1020 ?

In fact, is it possible to make the TAS1020 transparent USB to AC97 interface for the OS (windows or linux) ?

 

Thanks

Regards

Matthieu Baque