This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3101EVM-K: Asking for the ADC3101 GUI installation on Win10

Part Number: TLV320ADC3101EVM-K


Hi Team,

I would like install ADC3101 on my WIN10 OS. however, it will show the following message.

Can you please provide your suggestion?

BR,

SHH

  • Hi, Scott,

    The error suggests that the version of NI VISA driver you have is not compatible with the tool. When you execute  the ADC3101 installer, an older version of NI visa drivers is installed, this version may not be compatible with newer OS so you will need to download the latest version. You will need to uninstall the NI Visa drivers from your computer and then, download the latest  version from NI website. Then, execute the ADC3101 installer. You should  notice a message indicating that the NI visa driver will not be installed as you have a more recent version.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer