Other Parts Discussed in Thread: TPA3131D2
Hi all,
After doing some current consumption tests on TPA3131D2 eval board, I have measured a quiescent current that is not in line with the numbers on the datasheet.
The quiescent current was measured using the eval board with no load connected to the output. The result was 32mA with 7.4V PVCC.
According to the datasheet, at 7.4V PVCC with no load or filter, the quiescent current typically is 16mA, half of what we have measured.
Last revision of the datasheet was in Jan 2015, I don’t know if numbers have changed in further revisions.
In the datasheet there is no info about max values but usually if no info is provided, max values is about 5-10% higher than type values at room temperature.
Could someone confirm to me the datasheet values or point me to the right direction?
Regards,
Fran