Hi Sir
Could I connect VDD(Pin21), VCCL(Pin27), VCCR(Pin30), Vccp(Pin2) together ? when I use bus power mode
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Kai,
When the PCM2707C is operated in bus-powered mode, the required power supplies are generated on-chip and only a decoupling cap is required. Altough the voltage of the supplies you mention is the same, it is not recommended to connect them together, only a decoupling cap should be placed on each of those pins.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer