This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5717: Asking for the TAS5717 output power requirement

Part Number: TAS5717

Hi Team,
Can TAS5717 support output power 1Watt under 8ohm and PVDD 5V case?

BR,
SHH

  • SHH,

    This seems possible but let me double check and get back to you.

    Regards,

    -Adam
  • SH,

    I cannot confirm 100% as the datasheet does not show as low as 5V in the PVDD vs output power plot. I did try this on my EVM and I was able to get 1W of power into BTLx1 at 8 ohms at 5.25V. This is only one sample so not representative of all devices but it should follow.

    Regards,

    -Adam