Hello,
I have a problem with the TAS3251 and I configure it according to my settings, which I tested with the evaluation board before. Then I send data via I2S. However, I don't get any audio output at the output, which works fine with the Eval Board. When I measure at the DAC output, I see only a very short signal after the reset amp pin is pulled to high level. Afterwards nothing changes here anymore.
Do you have an idea where that could lie? Are there any registers that I can evaluate or what I can control?
The circuit is connected to the evaluation board and controlled several times. However, I got some of the first samples...
With kind regards,
Simon