Hi Sirs,
Customer would like change TI TAS5782M from I2S slave mode to I2S master mode for generate SCLK and LRCLK from TAS5782M.
We refered to datasheet chapter 9.3.3.1 and set below register to config TAS5782M:
Register Value
============
0x00 0x00
0x7f 0x00
0x02 0x11
0x01 0x11
0x09 0x11
0x0c 0x00
0x0c 0x03
0x0e 0x30
0x1c 0x1f
0x20 0x0f
0x21 0x1f
0x02 0x00
The MCLK came from host SAI interface(24.576MHz), after write above register, we can see SCLK(1.536MHz) and LRCLK(48KHz) send out from TAS5782M.
When customer played music from the host side, we can see the data(SAI_TXD) transmit from host to TAS5782M SDIN, but there is no signal arrive to speaker.
Would you please review if there is any missing to bring up TAS5782M in I2S master mode?
Thanks a lot
Wayne Chen
07/25/2018