Part Number: PCM2702
Other Parts Discussed in Thread: PCM2912A
sir,
The suggested IC(PCM2912A) is costly.Is there any other IC with less price and same spec.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Sayali,
All of or USB-audio codecs and DACs support up to 48KHz. As mentioned, we don't have a device with same features as PCM2912A and lower price. We have other PCM USB audio codecs, which have a lower cost but are slightly different than the PCM2912A. These parts supports two line input signals and don't support direct connection with microphones, so a pre-amplification stage should be used (which will increase cost).
Best Regards,
-Diego Meléndez López
Audio Applications Engineer