This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS3251: Delay sample possibility ?

Part Number: TAS3251


I look at an active speaker 1.1 configuration with Woofer and Tweeter. In the TAS3251 datasheet, I do not see a DSP option do delay samples on one channel. This is an option described in SLAU577A Using the TAS5754/6M and PCM5242 HybridFlow Processor (Rev. A)

This is described in section 7.6 :

HybridFlow 3 offers a Delay Select in series with Channel A. This allows time aligning Channel A with Channel B due to the delay associated with PBE and DBE processing only available with Channel B. Channel A can be delayed by up to 16 samples.
Has TAS3251 this feature ?
Best regards,
JMF