Part Number: DRV603
Hi all
Would you mind if we ask DRV603PW?
The customer consider using this device with Figure 13 configuration.(as second differential amplifier)
DRV inputs connect to DAC output.
DAC's offset is 2.5V.
<Question>
The customer would like to use this device with DC-Coupling which there is no C3 capacitance on Figure13.
Is it possible to configure with this condition?
If it occurs offset at DRV603's output, the customer plans to remove offset at DC cut circuit.
If it occurs any performance degradation, could you let us know?
Or, is this device only fitable for AC-coupling?
(In case of DC-coupling, it will be out of warranty?)
Kind regards,
Hirotaka Matsumoto