Hello,
I'm using the host interface to do pairing on a slave via NWM_DO_JOIN with a 10 second timeout, device ID = 0xFFFFFFFF, and all other IDs set to zero. The slave successfully pairs with a master. However, the Network LED does not output the PAIRING LED pattern before I enable pairing on the master. The network LED just displays the ALONE LED pattern. After pairing completes, the slave Network LED outputs the ACTIVE LED pattern.
Shouldn't I see the PAIRING LED pattern while NWM_DO_JOIN is executing? I was expecting the double blink pattern that the development kits output on the LED after you push the pairing button.
Thanks,
Kurt