This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2706/7 Drivers and I2S input capability

Other Parts Discussed in Thread: PCM2706, DIT4096, PCM2902B

Is there support for Windows CE6 for the PCM27xx series devices?  Also, is I2S input possible for the PCM2706/7 device so that bi-directional communication can be enabled?

  • Tara,

    The PCM2706/7 does not support routing the I2S input to the USB.  I would recommend using:

    TUSB3200A - USB Streaming Controller - This can be used to route audio between USB and I2S, both directions.
    PCM177x - DAC with HP/Line-Out, connects to the TUSB3200A via I2S.
    DIT4096 - Digital Audio Transmitter - Converts I2S to S/PDIF for optical or coaxial audio out

    Let me know if you have any quesitons.

    Thanks,
    Brian

  • Tara,

    Also take a look at the PCM2902B as a possible substitute to the PCM2706 or PCM2707.  It doesn't have I2S, but it does have S/PDIF digital input and output to USB.

    Thanks,
    Brian